TGML Text Value Conversion: <ConvertText>

ConvertText specifies how a server variable (signal) value is to be converted to a TGML element attribute value. ConvertText assumes that the signal value is a text. A ConvertText element belongs to the immediate parent Bind element.

A ConvertText rule is executed when the signal value matches the specified text (SignalEqualTo).

Attribute Type Description

AttributeValue

String (untyped)

The attribute value that is to be set (resulting value). The type is determined by the bound Attribute (referenced by the Bind element).
Inheritable: No
Animatable: No

SignalEqualTo

String (untyped)

Corresponds to "="
Inheritable: No
Animatable: No